AXIS#.VL.LIMITP

Description

AXIS#.VL.LIMITP sets the velocity command positive limit.

If the input to the velocity loop is higher than AXIS#.VL.LIMITP, then the actual velocity command AXIS#.VL.CMD is limited by the value of AXIS#.VL.LIMITP.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

30,000 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

See Also

AXIS#.VL.LIMITN, AXIS#.VL.CMD

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.LIMITP

5011h

06h

Unsigned32

Velocity

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6032

1

6032 (0x1790)

AXIS1.VL.LIMITP

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.VL.LIMITP

6032

Float

Read/Write

Velocity